cancel
Showing results for 
Search instead for 
Did you mean: 

why are vbat, vrefint and temp ADC3 channels on STM32H7 no longer available on the latest CubeMx version? I'm I missing another conifguration to make them available?

Sebastiain Fernandez
Associate II

screenshot from an .ioc file created with an earlier version of CubeMx

CubeMx version 5.30

0690X00000BxBm3QAF.png

screenshot from an .ioc file created with CUbeMx version 5.5.0

0690X00000BxBnLQAV.png

Full details of installation:

STM32CubeMX - STM32 Device Configuration Tool

Version: 5.5.0-RC6

Build: 20191220-1511 (UTC)

Copyright (c) 2018 STMicroelectronics. All rights reserved

STM32CubeIDE

Version: 1.2.1

Build: 5190_20200115_1224 (UTC)

(C) 2019 STMicroelectronics ALL RIGHTS RESERVED

Thanks

4 REPLIES 4
Khouloud ZEMMELI
ST Employee

​Hello @Sebastiain Fernandez​ ,

Issue has been fixed , the fix will be available in the next release.

Best Regards,

Khouloud

Sebastiain Fernandez
Associate II

Thanks

Sorry if this question had been answered before I didn't find any conversations related to the issue

Best Regards

​not problem you're always welcome

Sebastiain Fernandez
Associate II

Hi I just found that the problem is in fact related to the STM32CubeH7 firmware package 1.6.0.

I downgraded to version 1.5.0 with CubeMx 5.5.0 and the ADC3 vbat, temp and vrefint channels are available

Best regards