2019-03-24 3:55 PM
2019-10-05 1:05 PM
USE_HAL_UART_REGISTER_CALLBACKS is very important settings. Should be added to CubeMX!!!
2019-10-05 10:09 PM
Well, as there is no "global.h" probably in the project settings/compiler/options where you can add compile options.
Hardly portable across IDE solution.
2020-02-03 11:50 PM
It is defined (to 0 as default) in the file stm32h7xx_hal_conf.h
2021-02-10 2:32 AM
Hello, i found your awnser.
In CubeMX, go to "Project manager", in the left side you will see "Advanced Settings".
if you go over there, you can see all Register Callbacks on the right side. They are all disabled my default, you can eable them there.
GL ^^
Angus