cancel
Showing results for 
Search instead for 
Did you mean: 

When STM32CubeMX generating user source code it's just stuck

Eduard Ch
Associate
Posted on March 11, 2017 at 19:02

Sometimes, STM32CubeMX just stuck at generating code, and i am not able to do anything. Just end the process from Task Manager. What does happen?

P.S. Jawaw.exe in the Task Manager not load my CPU at all.

#stm32cubemx
2 REPLIES 2
Nesrine M_O
Lead II
Posted on April 03, 2017 at 17:52

Hi

drsnail

,

  • Could you please precise the MX version with it you have found the issue?
  • is this a recurrentissue or faced only one time?
  • you have found the issue when migrating an old project from one MX version to another version (example from 4.16 to 4.20)? if yes please precise the MX versions.

-Nesrine-

MH Huang
Associate
Posted on April 09, 2018 at 21:10

Hi,@Nesrine M_O

I have also this issue. The cubeMX hangs in the phase of ''generating user code''

I am using STM32CubeMX(4.25.0) as plug-in under Eclipse Oxygen.3(4.7.3) with Windows 10

I tried at least 5 time, I got no success.

This is my first experience using STM32CubeMX, I have no comparison with previous version.

This is the info for my project

Chip: STM32F103C8

RCC, HSE: Crystal

USB: Enabled

USB_DEVICE, IP: CDC

0690X0000060AS5QAM.png0690X0000060ARvQAM.png0690X0000060AV3QAM.png0690X0000060AKWQA2.png