Associate II
November 29, 2022
Question
What happens to FreeRTOS code generation?
- November 29, 2022
- 8 replies
- 3368 views
Today my STM32CubeIDE does an update to the Version: 1.11.0 (Build: 13638_20221122_1308 (UTC) ) including the CubeMX Version: 6.7.0-RC2 (Build: 20221118-1646 (UTC))
Using the FreeRTOS Middleware the generation of the main file has a big bug. There will be the "USER CODE Header" lines instead of the FreeRTOS lines inseide the main()-function.
This happens also if I create a new empty project using the FreeRTOS middleware. It will generate the attached main-c-file. See lines 145-151.
I haven't searched where the bug comes from.