2020-03-09 03:01 AM
This just looks like a comment but it seems a code outside these comment have different affect.
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
Solved! Go to Solution.
2020-05-18 09:33 AM
I have found the answer to myself.
The user code sections that are between two comment lines are dedicated to write the code inside the lines. Anycode written outside of these sections will be removed in case of anychange at CubeIDE interface (*.ioc)
2020-05-18 09:33 AM
I have found the answer to myself.
The user code sections that are between two comment lines are dedicated to write the code inside the lines. Anycode written outside of these sections will be removed in case of anychange at CubeIDE interface (*.ioc)