2019-09-16 5:04 AM
Hello
In the PC app, I work with the STM32F722RETx LQFP64 micro-controller
In WIN7 it always works. At WIN10 does not work.
After I turn off and turn on the card, the board data that the system sees (both win7 and win10) is:
Status for device COM2 :
-----------------------
Baud: 1899758337
Parity: None
Data Bits: 242
Stop Bits: 1
Timeout: OFF
XON/XOFF: OFF
CTS handshaking: OFF
DSR handshaking: OFF
DSR sensitivity: OFF
DTR circuit: OFF
RTS circuit: ON
At win10 it doesn't work
On win7 the board works after my app on win7, where I set the COM parameters
the system starts to work (on both win7 and win10):
Status for device COM2 :
-----------------------
Baud: 9600
Parity: None
Data Bits: 8
Stop Bits: 1
Timeout: ON
XON/XOFF: OFF
CTS handshaking: OFF
DSR handshaking: OFF
DSR sensitivity: OFF
DTR circuit: OFF
RTS circuit: ON
I move the board (which is still ON) to win10 and it works
After the shutdown, it stops working at win10 again
It seems that the data is stored on the board only until the board is ON
This is the USB configuration on STM32CubeMX
Please help us to solve the problem
Thanks
Solved! Go to Solution.
2020-01-13 6:44 AM
answer for every one having the same problem:
in file usb_cdc_if.c add the following USBD_CDC_LineCodingTypeDef
USBD_CDC_LineCodingTypeDef LineCoding =
{
115200, /* baud rate*/
0x00, /* stop bits-1*/
0x00, /* parity - none*/
0x08 /* nb. of bits 8*/
};
In function CDC_Control_FS/ CDC_Control_HS
add to these two cases the code bellow:
case CDC_SET_LINE_CODING:
LineCoding.bitrate = (uint32_t)(pbuf[0] | (pbuf[1] << 8) | \
(pbuf[2] << 16) | (pbuf[3] << 24));
LineCoding.format = pbuf[4];
LineCoding.paritytype = pbuf[5];
LineCoding.datatype = pbuf[6];
break;
case CDC_GET_LINE_CODING:
pbuf[0] = (uint8_t)(LineCoding.bitrate);
pbuf[1] = (uint8_t)(LineCoding.bitrate >> 8);
pbuf[2] = (uint8_t)(LineCoding.bitrate >> 16);
pbuf[3] = (uint8_t)(LineCoding.bitrate >> 24);
pbuf[4] = LineCoding.format;
pbuf[5] = LineCoding.paritytype;
pbuf[6] = LineCoding.datatype;
break;
2020-01-13 6:44 AM
answer for every one having the same problem:
in file usb_cdc_if.c add the following USBD_CDC_LineCodingTypeDef
USBD_CDC_LineCodingTypeDef LineCoding =
{
115200, /* baud rate*/
0x00, /* stop bits-1*/
0x00, /* parity - none*/
0x08 /* nb. of bits 8*/
};
In function CDC_Control_FS/ CDC_Control_HS
add to these two cases the code bellow:
case CDC_SET_LINE_CODING:
LineCoding.bitrate = (uint32_t)(pbuf[0] | (pbuf[1] << 8) | \
(pbuf[2] << 16) | (pbuf[3] << 24));
LineCoding.format = pbuf[4];
LineCoding.paritytype = pbuf[5];
LineCoding.datatype = pbuf[6];
break;
case CDC_GET_LINE_CODING:
pbuf[0] = (uint8_t)(LineCoding.bitrate);
pbuf[1] = (uint8_t)(LineCoding.bitrate >> 8);
pbuf[2] = (uint8_t)(LineCoding.bitrate >> 16);
pbuf[3] = (uint8_t)(LineCoding.bitrate >> 24);
pbuf[4] = LineCoding.format;
pbuf[5] = LineCoding.paritytype;
pbuf[6] = LineCoding.datatype;
break;