2024-08-19 09:44 AM
Hello,
I am currently experiencing issues with compiling a Makefile project for the STM32F103C8T6, generated by STM32CubeMX. The project has the FreeRTOS middleware enabled, with CMSIS V2.
Compilation of the generated code results in these errors:
I believe the first error has something to do with a missing symbol/definition for CMSIS_device_header, but I am unsure as to which header file should be there instead. The other error seems to be a configuration error, but I, once again, have no idea what to do to fix it.
It's also worth noting that I was able to generate a project with the same settings and compile it previously. I don't recall tampering with anything that could have caused this breakage.