UART only receive one byte
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-08 4:16 PM
I'm trying to receive more than 1 byte but it receive only 1 byte. Poll method or IT, it doesn't matter. Always receives 1 byte and writes it in rx_buffer[0]. When I search it I found out the reason is timeout, I increase timeout 1000 from 100ms but nothing changes. Can anyone help me please?
Here is my code for poll
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "string.h"
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart6;
DMA_HandleTypeDef hdma_usart1_rx;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART6_UART_Init(void);
USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
char rx_buffer[50];
char tx_buffer[50];
while (1)
{
HAL_UART_Receive(&huart1,(uint8_t*)rx_buffer,4,1000);
memcpy(tx_buffer,rx_buffer,4);
HAL_UART_Transmit(&huart6,(uint8_t*)tx_buffer,strlen(tx_buffer),1000);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
Solved! Go to Solution.
- Labels:
-
DMA
-
STM32CubeMX
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-16 2:20 AM
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "string.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart6;
DMA_HandleTypeDef hdma_usart1_rx;
DMA_HandleTypeDef hdma_usart6_tx;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART6_UART_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
#define rx_buff 512
#define main_buff 2048
uint8_t rx_buffer[rx_buff];
uint8_t main_buffer[main_buff];
uint16_t oldPos;
uint16_t newPos;
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
if (huart->Instance == USART1)
{
oldPos = newPos; // Update the last position before copying new data
if (oldPos+Size > main_buff) // If the current position + new data size is greater than the main buffer
{
uint16_t datatocopy = main_buff-oldPos; // find out how much space is left in the main buffer
memcpy ((uint8_t *)main_buffer+oldPos, rx_buffer, datatocopy); // copy data in that remaining space
oldPos = 0; // point to the start of the buffer
memcpy ((uint8_t *)main_buffer, (uint8_t *)rx_buffer+datatocopy, (Size-datatocopy)); // copy the remaining data
newPos = (Size-datatocopy); // update the position
}
/* if the current position + new data size is less than the main buffer
* we will simply copy the data into the buffer and update the position
*/
else
{
memcpy ((uint8_t *)main_buffer+oldPos, rx_buffer, Size);
newPos = Size+oldPos;
}
/* start the DMA again */
HAL_UARTEx_ReceiveToIdle_DMA(&huart1, (uint8_t *) rx_buffer, rx_buff);
__HAL_DMA_DISABLE_IT(&hdma_usart1_rx, DMA_IT_HT);
HAL_UART_Transmit_DMA(&huart6,rx_buffer, sizeof(rx_buffer));
}
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART1_UART_Init();
MX_USART6_UART_Init();
/* USER CODE BEGIN 2 */
HAL_UARTEx_ReceiveToIdle_DMA(&huart1, rx_buffer, rx_buff);
HAL_UART_Transmit_DMA(&huart6, rx_buffer, sizeof(rx_buffer));
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-16 9:06 AM
From what i see, main_buffer is pointless as you are not doing anything with it.
My UART2 is your UART1 and my UART1 is your UART6 which this is working on a Nucleo-L432 board
uint8_t tx_buffer[rx_buff];
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
if (huart->Instance == USART2)
{
/* start the DMA again */
memset(&tx_buffer, 0, sizeof(tx_buffer)); // clear tx buffer
memcpy(&tx_buffer, &rx_buffer, Size); // copy only what was received
HAL_UART_Transmit_DMA(&huart1, tx_buffer, Size); // use Size instead of sizeof(rx_buffer)
HAL_UARTEx_ReceiveToIdle_DMA(&huart2, (uint8_t *) rx_buffer, sizeof(rx_buffer));
}
}
Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!
If you find my solution useful, please click the Accept as Solution so others see the solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-16 5:13 PM
Thank you so much!!!! It works!!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-16 8:43 PM
You're welcome! Can you please select as best answer?
Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!
If you find my solution useful, please click the Accept as Solution so others see the solution.

- « Previous
-
- 1
- 2
- Next »