UART DMA race condition bug
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-26 11:06 PM
Hi, I want to discuss this problem in UART DMA on STM32F4 boards
I am sorry to upload picture rather than code.
Moreover, my English is not proficient and please understand.
I tested my code under nucleo-f429zi.
-------------------------------------------
First of all, I configured UART3 with DMA option on board.
The below figure is the code I tested
I thought that if I called UART_Receive_DMA function in the code, the data only receive DMA method.
The reason is that UART_Start_Receive_DMA() called by HAL_UART_Receive_DMA() make receiver state (RxState) HAL_UART_STATE_BUSY_RX in line 3259 of second picture.
So when I called HAL_UART_Recevie() which does not use DMA method, HAL_UART_Recevie() cannot receive any data if HAL_UART_Receive_DMA() is already called before HAL_UART_Recevie().
This is because HAL_UART_Recevie() can receive data when receiver state is free (RxState == HAL_UART_STATE_READY) (below figure 1271 line)
So I thought that if user makes the RxState HAL_UART_STATE_READY after calling HAL_UART_Receive_DMA(), HAL_UART_Receive() could work (below figure)
I tested this code and result is weird.
When I give input string "Hello world!!" via serial communication to UART, UART cannot receive first character of the input string.
I think that the problem is HAL_UART_Receive_DMA() and HAL_UART_Receive() only check once receiver state (RxState) and both functions are ready to receive data.
So this code may make race condition between both functions.
I want to hear your opinion about this.
- Labels:
-
STM32F4 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-27 3:44 AM
Mixing DMA and not DMA is not such a good idea.
Below a simple demo that sends data and reads data from another device such as a PC.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-27 5:39 AM
You can't have HAL_UART_Receive() and HAL_UART_Receive_DMA() working simultaneously. The peripheral has a single receive lane, and both of these functions use it. As you saw, the functions will return HAL_BUSY if one of them is already working.
> So I thought that if user makes the RxState HAL_UART_STATE_READY after calling HAL_UART_Receive_DMA(), HAL_UART_Receive() could work (below figure)
This is nonsense. Forcing the state to reflect something else, just so a function returns HAL_OK, doesn't get around the underlying limitation of a single receive lane.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-28 2:09 AM
Hello @Taehyun92039203.
Thank you for posting and welcome to the ST Community.
I advise you to take a look at this ST Lab: STM32CubeMX basics: 10.11 STM32Cube HAL labs UART - UART DMA - YouTube.
The video explains how to use the UART with DMA using STM32F4 boards.
You can also consult this wiki: Getting started with UART - stm32mcu.
Thank you.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.