2025-12-10 11:26 AM
The erroneous configuration in the tx_initialize_low_level.S is this:
LDR r1, =0x40FF0000 // SysT, PnSV, Rsrv, DbgM
The tx_initialize_low_level.S file is generated upon selecting ThreadX 'Core' in the STM32CubeMX v6.15.0, and the above line is thereafter never changed. Specifically, upon enabling 'Enable BASEPRI support' and selecting a very common value of 5 for the TX_BASEPRI_VALUE, the above line is not updated accordingly. Not syncing the SYSTICK IRQ priority with the TX_BASE_PRI_VALUE of course leads to a system failure.
This issue can be duplicated by creating a brand new project with STM32CubeMX v6.15.0 and it can be seen in the sample projects included in the Applications/ThreadX in the STM32Cube_FW_U5_V1.8.0
2025-12-26 3:05 PM
@Pavel A. thanks for confirming my observation - I did specify line 149 in my post above, so I was very confused by the response from @Mahmoud Ben Romdhane Anyway, it was beside the point since I didn't realize that I could "fix" the code-generation problem of always overwriting my local fix by simply patching my local copy to the ST library code - for some reason I was assuming that the assembly file was being uniquely generated by CubeMX instead of just copy and pasted from the library.
2026-01-08 8:01 AM
Hello @ScottyWinsome
Further to the first issue, I used an example provided through STM32CubeMX Data Base, Tx_Thread_Creation with Nucleo-U5A5ZJ-Q.
The tasks are well executed even if I enable BASEEPRI and set the TX_BASEPRI_VALUE to 5.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.