cancel
Showing results for 
Search instead for 
Did you mean: 

STM3N6: CubeMX pin conflicts (false positives)

svogl
Associate III

Hi all, 
I am trying to get a zephyr project running on an STM32N6570-DK, including Camera, NPU, VENC and Ethernet.

I have been using STMCubeMX 6.16.1 to create the project based on the provided DK default settings.

For the Ethernet block, the configurator shows pin conflicts, I double-checked and the pins are not in use by the Ethernet driver:

svogl_0-1767880253394.png

There are similar warnings for the SD/MMC2 block:

svogl_1-1767880552958.png

Am I missing something here or can it safely be ignored? 

Simon

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

These can be safely ignored. The presentation isn't the best, but the UI is telling you that some things can't be enabled because some pins are in use. But there is no error with the current settings.

If you open the dropdown, you will see only some settings within there have issues.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Super User

These can be safely ignored. The presentation isn't the best, but the UI is telling you that some things can't be enabled because some pins are in use. But there is no error with the current settings.

If you open the dropdown, you will see only some settings within there have issues.

If you feel a post has answered your question, please click "Accept as Solution".
svogl
Associate III

great, thanks for the quick response!
Simon

Hi @svogl and @TDK ,

Thank you very much - the STM32Nxx7 is an extremely advanced and complex chip so it's a help to know that these warnings can be ignored.

Will