2020-02-22 8:36 AM
When the file stm32f3xx_hal_msp.c is created there is a missing line in function void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc) which enables the DMA clock - ( __HAL_RCC_DMA1_CLK_ENABLE();
The STM32CubeMX generates code that enables that clock in main.c in a separate function called MX_DMA_Init(); But this is to late to configure DMA and make it work.
So with that extra line in HAL_ADC_MspInit everything is fine. Can you please fix that problem and offer an update so that everything works just out of the box.
PS: I really appreciate the STM32CubeMX. It is very handy
2020-03-09 3:46 AM
Hello @HMay.1 ,
Which STM32CubeMX version are you using? This issue should be already fixed with the version 5.5 of the tool, currently we are on version 5.6.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-03-13 4:20 AM
Hello Amel,
thanks for the reply. The version i am using is indeed version 5.4. But when i click on Help->Check for update the program tells me that everything is up to date. But this is another topic. I am glad you have fixed that issue.
regards
Hendrik
2020-05-23 5:12 AM
Hello I may have the same problem with G4.
It does not include DMAx_CHANNELx_CLK_ENABLE();.