cancel
Showing results for 
Search instead for 
Did you mean: 

The project of stm32h7 dual-core which using keil can't save project settings.

JTOM.1
Associate II

The project of stm32h7 dual-corewhich using keil can't save project Settings.

It is restored to the default settings when using cubemx to regenerate the Keil project each time.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Khouloud ZEMMELI
ST Employee

​Hello @JTOM.1​ 

Could you please share your ioc file and specify which setting has not been saved?

Thanks

Khouloud

all of the options in keil can not be saved. compiler options ,linker options,debug options,etc.

The keil version which I use is 5.31.