cancel
Showing results for 
Search instead for 
Did you mean: 

The CubeMX/CubeIDE login issue is resolved

Semer CHERNI
ST Employee

Hello CubeMX/CubeIDE users. 

From the time period of May 14 to May 17, 2024, some users have faced issues when connecting to the ST network while using CubeMX or CubeIDE.
Some examples were issues downloading firmware packages using STM32CubeMX and STM32CubeIDE tools, or logging in to myST through the software.

The misbehavior in one of our servers that lead to the failed connection attempts was identified and fixed. The login mechanism is now working as expected.

We apologize for the inconvenience faced by all the CubeMX/CubeIDE users.

In case of login or download issue, we refer to the following article on how to set the “Network connection” for the tools: How to set the network connection parameters for STM32CubeIDE

If you still face issues, contact us or reply to this post so we can provide support.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0