2019-03-25 10:36 AM
Bug Report STMCubeMX 5.1.0
The tool does not load the timer configuration correctly when channel 4 is "Input Capture direct mode" and channel 3 is "Input Capture indirect mode".
After loading a configuration with these settings channel 3 is set to "Disable". Happens for timer 2 and timer 3.
Attached are a ioc file and a screenshot from the timer configuration.
2019-03-26 12:28 AM
Hello @sielenk
Thank you for the feedback, this is reported internally for further check.
Best Regards,
Khouloud.
2019-03-31 07:19 AM
Workaround:
Does not happen when Pin Stacking is disabled.
I had the timer and GPIO inputs enabled for the same pin.