2015-05-05 9:38 AM
Hello,
Seems to be a bug in ADC configuration. Behaves that some range of ranks are missing at the beginning. Steps to reproduce a bug: - Set ''Number of conversion'' to for example 14 - Now we have proper number of ranks, enumerated 1,2,3,...,14 - Save the file, close, reopen - Open ADC configuration - We can see there are missing ranks 2,3,4 I also found a workaround for the bug: if we see that some range of ranks is missing we can set number of ranks to 1, click apply, then once again set proper number of ranks and seems to be working after project reload. BR, Michal #stm32cube #cubemx #stmcube-stmcubemx-cube-stm32cube2015-05-06 8:14 AM