STMCubeMX 4.7.1: Bug in ADC Configuration
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-05 09:38 AM
Posted on May 05, 2015 at 18:38
Hello,
Seems to be a bug in ADC configuration. Behaves that some range of ranks are missing at the beginning. Steps to reproduce a bug: - Set ''Number of conversion'' to for example 14 - Now we have proper number of ranks, enumerated 1,2,3,...,14 - Save the file, close, reopen - Open ADC configuration - We can see there are missing ranks 2,3,4 I also found a workaround for the bug: if we see that some range of ranks is missing we can set number of ranks to 1, click apply, then once again set proper number of ranks and seems to be working after project reload. BR, Michal #stm32cube #cubemx #stmcube-stmcubemx-cube-stm32cube
Labels:
- Labels:
-
STM32Cube MCU Packages
-
STM32CubeMX
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-06 08:14 AM
Posted on May 06, 2015 at 17:14I've seen the same behavior for the last few versions... and it generated bad init code when not displaying all ranks. Your workaround didn't help me in older versions. Fingers crossed that it has improved in 4.7.1. I started hand editing the project file to correct the problem.
![](/skins/images/9117C6B72C9F598A212AA17633C1CC28/responsive_peak/images/icon_anonymous_message.png)