2014-10-20 2:39 AM
I had CubeMX installed and working fine. Then I updated the application and now all I see is dialog flashing by the says ''Check files''. After that nothing happens.
When I start it from a DOS box I get: java -jar STM32CubeMX.exe HeapMemory: 16252928 Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM 32CubeMX Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM 32CubeMX loadPluginJar : clock loadPluginJar : add clock loadPluginJar : filemanager loadPluginJar : add filemanager loadPluginJar : ipmanager loadPluginJar : add ipmanager loadPluginJar : pinoutconfig InternalPropertyChange: ChangeKeepUser dont care loadPluginJar : add pinoutconfig loadPluginJar : power loadPluginJar : add power loadPluginJar : projectmanager This is Windows This is 32 Bit VM C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\\db\plugins\projectman ager\windows\32\toolgen.dll loadPluginJar : add projectmanager loadPluginJar : updater Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM 32CubeMX STM32CubeMX Software Update Start Now I have reinstalled the program with the same result. Suggestions? #stmcube-stmcubemx-cube-stm32cube2014-10-20 3:06 AM
I have the same problem.
2014-10-20 11:46 PM
Hi !
I have the same problem on Windows7 & 8 64bits with clean and update installation of CubeMx.What can be problem ?2014-10-21 3:01 AM
I have same problem and I don't understand why...
2014-10-22 6:28 AM
I also have the same problem.
2014-10-22 8:10 AM
I tried this: in my documents folder I found an .stm32cube folder and I deleted it. Re-installed last version of CubeMX and works fine (till now)
2014-10-23 3:39 AM
Thank you!
That helped.2014-10-23 4:26 AM
It helped
me
also
.Thanks
2014-11-19 6:33 AM
Can you please indicate which version you started from and which version you upgraded to.
Thank you.2014-11-19 7:27 AM
I had this problem when updating from 4.3 to 4.4. The update from 4.4 to 4.5 today was OK.