cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 raw LwIP ping - not working

Attila
Associate II

Hi everyone,

I have an STM32H743 Nucleo kit with ethernet interface. I'm trying to make alive a simple TCP/IP demo with the raw LwIP stack. I'm using STM32CubeMX with TrueStudio.

In the Cube I have configured the followings:

- Clock is set to th highest at every bus

- PHY is set to LAN8742. IOs are configured by Cube to their special function

- MPU is not used, nor cache (I and D also set to off)

- LwIP is used without FreeRTOS

- Ethernet IRQs are enabled in the Cube

- DHCP, ICMP, UDP enabled in the settings of the LwIP

In the TrueStudio project:

- I have modified the linker to place ETH_DMADescTypeDef DMARxDscrTab, ETH_DMADescTypeDef DMATxDscrTab and Rx_Buff into the D2_RAM at the mentioned addresses

- I have call the MX_LWIP_Process() in the main/while(1)

With these settings, I'm still not seeing my device on my network (I have tried WireShark also). What else do I miss to be able to ping it?

Thank in advance for any kind of idea!

Best regards,

Attila

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello,

Please follow in this discussion the recommendation and generate code to run the LWIP on STM32H7.

Then, keep us informed about yout progress.

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
User.103
Associate

Have you configured your cache?