cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 VREFBUF wrong voltage in CubeMX GUI CubeIDE 1.6.1

Remon Dijkstra
Associate II

CubeMX lets you choose 4 voltages.

Option/Value 0 should be 2.5V jnstead of the mentioned 2.048V

Option/Value 1 should be 2.048 instead ogf the mentioned 2.5V

Proof: When you select 2.5V it generates 2.048 on the VREF output.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Dear Remon,

It seems that each of couples SCALE0/SCALE1 and SCALE2/SCALE3 are swapped.

This will be escalated to be fixed in coming revisions of CubeMx.

Thank you.

STM32

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Dear Remon,

It seems that each of couples SCALE0/SCALE1 and SCALE2/SCALE3 are swapped.

This will be escalated to be fixed in coming revisions of CubeMx.

Thank you.

STM32

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.