2022-04-06 10:42 PM
Hi,
I've found three bugs in CubeMX for the DCMI code generation.
uC: STM32H7A3IITxQ
CubeMX Version: 6.5.0
Firmware Package: STM32Cube FW_H7 V1.10.0
The IOC-file is attached.
1.Following lines are getting generated in HAL_DCMI_MspDeInit:
HAL_DMA_DeInit(dcmiHandle->DMA_Handle);
HAL_DMA_DeInit(dcmiHandle->hdmarx);
HAL_DMA_DeInit(dcmiHandle->hdmatx);=> The dcmiHandle has no members named "hdmarx" and "hdmatx". (Compile Error)
2.Following lines are getting generated in HAL_DCMI_MspInit:
__HAL_LINKDMA(dcmiHandle,DMA_Handle,hdma_dcmi_pssi);
__HAL_LINKDMA(dcmiHandle,hdmarx,hdma_dcmi_pssi);
__HAL_LINKDMA(dcmiHandle,hdmatx,hdma_dcmi_pssi);=> Same thing here, "hdmarx" and "hdmatx" are no members of the dcmiHandle. (Compile Error)
3.In the main function, following lines are getting generated:
MX_GPIO_Init();
MX_FMC_Init();
MX_DCMI_Init();
MX_DMA2D_Init();
MX_LTDC_Init();
MX_TIM2_Init();
MX_I2S1_Init();
MX_I2C1_Init();
MX_I2C2_Init();
MX_SPI2_Init();
MX_CRC_Init();
MX_DMA_Init();
MX_JPEG_Init();
MX_TIM7_Init();
MX_TouchGFX_Init();=> MX_DMA_Init() has to be called before MX_DCMI_Init(), else the DCMI-Peripheral isn't working.
Two years ago, someone reported the same problem: https://community.st.com/s/question/0D50X0000BvhrT2SQI/why-do-i-get-overrun-error-when-using-dcmi?t=1648534322363
Hope this get's fixed soon, as I have to change these lines everytime i regenerate the code with CubeMX.
2023-07-14 7:14 AM
Hi @Florian Moser ,
Could you please check using latest STM32CubeMX version (6.9.0)? Is the same issue still faced?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.