2021-09-22 3:18 AM
When creating a new Freertos Task like this:
osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes);prvAddNewTaskToReadyList(...)will be called and uses
taskENTER_CRITICAL()to disable interrupts. This breaks down to the call of void vPortEnterCritical( void )
void vPortEnterCritical( void )which increases uxCriticalNesting by one.
Before leaving
void vPortExitCritical()is called. This function should decrease uxCriticalNesting and reactivate interrupts if uxCriticalNesting == 0.
However, uxCriticalNesting was previously initialized with 0xaaaaaaaa. So that uxCriticalNesting == 0 is not reached.
A later call of
osKernelStart();finally sets uxCriticalNesting to 0 and reactivates all interrupts.
This results in deactivated interrupts between the first task creation and kernel start, which has undesirable side effects such as the systick timer being stopped, which results in a broken HAL_Delay() function.
Solved! Go to Solution.
2021-09-30 2:55 AM
Hello @Mathieu Münch-zur Megede ,
This is intentional from the FreeRTOS maintainer. Please see this comment.
BeST Regards,
Walid
2021-09-30 1:34 AM
Hello @Mathieu Münch-zur Megede
This issue has been internally raised. I will keep you posted.
Thanks for your contribution.
BeST Regards,
Walid
2021-09-30 1:35 AM
Internal ticket number: 114615 (PS: This is an internal tracking number and is not accessible or usable by customers)
2021-09-30 2:55 AM
Hello @Mathieu Münch-zur Megede ,
This is intentional from the FreeRTOS maintainer. Please see this comment.
BeST Regards,
Walid
2021-09-30 7:40 AM
> systick timer being stopped, which results in a broken HAL_Delay() function.
Let's see. vPortEnterCritical executes vPortRaiseBASEPRI which is raises basepri to configMAX_SYSCALL_INTERRUPT_PRIORITY.
So, interrupts of priority greater than configMAX_SYSCALL_INTERRUPT_PRIORITY will work before the scheduler starts.
These interrupts cannot call FreeRTOS functions anyway.
Just use a different timer for the HAL tick, as recommended by CubeMX/CubeIDE. Set it's priority high.