2015-02-02 1:05 PM
I am using an STM32F051K6Txm device.
with STM32Cube FW_F0 V1.0.0. Setting the Sysclk to use HSE, but code generated is HSI. Attached is my ioc file. To make this work I had to edit theSystemClock_Config ()function and changed { RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInit; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI => must be RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; without this mod, the system is using the RC osc, and I have drifs so large that the Uarts stops working. Changing this line and the xtal osc can clearly be seen on the MCO port pin, and an frequency counter shows a 10-4 change. Thanks #hse-config #cubemx
2015-02-17 2:35 AM
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.