2016-12-24 12:51 PM
Using STM32CubeMX version 4.18.0 on Windows 10 Pro (build 1607) with an UHD (4K) display results in tiny toolbar icons and a very tiny Clock Configuration diagram. Please see attached screen capture image. Not that this application window is not maximized.
Is there any way to scale these images within the STM32CubeMX application so that I can see them with human eyes?
Additionally, the screen looks the same even when I drag the STM32CubeMX application to a different, lower-resolution monitor.
Any help would be appreciated.
Thanks,
Dale
#stm32cubemxSolved! Go to Solution.
2017-09-18 05:10 AM
This solution works perfectly on my system. In fact, it helps other
Windows apps that don't deal with high DPI displays as well.
Thank you very much!
Thank you,
Dale Wheat
(330) 732-5307
On Mon, Sep 18, 2017 at 3:06 AM, Teemu Ikonen <
2017-09-18 01:38 PM
This is extremely helpful! I'm quite surprised to find a months-old question with a solution just posted today. Thank you very much!
2017-09-19 05:47 PM
If the ST developers are not going to address this issue, then I think that they should publish this work-around with the installation notes. UHD displays are becoming more common these days and the software is quite difficult to use without this feature.
Are you listening, ST developers?
🙂
2017-10-06 02:15 AM
hello,i have a problem! my laptop display is 4k, when i want to run stmcube the icons are very small,my windows is 8.1.please help me, how can i fix it ? ,thank
2017-10-16 01:54 PM
Hi everyone, same problem! Hope to get a solution for this issue.