2017-03-23 11:28 PM
I'm trying to make a interrupt handler which doesn't use FreeRTOS function and preemption priority is higher than FreeRTOS, say 2.
However every time I load .ioc file, STM32CubeMX checks the 'Uses FreeRTOS functions' checkbox of the interrupt handler, so I need to uncheck it manually.
Please try with the attached .ioc file.
STM32CubeMX version is 4.20.0
STM32Cube FW_F7 V1.4.1
#stm32cubemx2017-03-24 05:36 AM
Hello,
Your issue is reported internally to our CubeMx team for further check.
You should use the last version of STM32CubeF7 firmware package which contains fix defect, enhancements and updates to new version of FreeRTOS V9.0.0
Imen
2017-04-27 06:00 AM
Hi
Sakurai.Hiroshi
,For your information, the issue you reported will be delivered in the next CubeMX release (4.21).
BR. Eric