2026-01-23 7:59 AM
I am using cubemx to generate a CMAKE project for a NUCLEO_144 based board (NUCLEO_H563).
Project generation creates a cmake/stm32cubemx/CmakeLists.txt file that generates a macro define "USE_NUCLEO_144".
it also auto creates a stm32h5xx_nucleo_conf.h file that also creates the same define:
Solved! Go to Solution.
2026-02-25 2:42 AM
2026-01-25 11:38 PM - edited 2026-01-28 2:36 AM
Hello @dvescovi
Thanks for highlighting this issue,
Our team are aware about this issue, and it will be fixed in the upcoming releases of STM32CubeMX (Ticket 222934 This is an internal tracking number and is not accessible or usable by customers.)
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-25 2:42 AM