2019-01-03 12:47 AM
Helloo,
Problem occured after updating STM32CubeMX from ver 4.x to ver 5.0.1. It was running perfectly before. But now, when I try to start it, nothing happens acceps my mouse icon turn into spinnnig icon for few seconds.
I did try to uninstall STM32CubeMX too. Bu STM32CubeMX software is not displayed in the programs list too. I tried using the uninstaller uninstaller.jar, but does not work too, does the same spinning mouse icon for few second but nothing else.
Please see the attached files.
I need an urgent help since I use STM32CubeMX actively....
Thanks a lot in advance.
2019-01-09 11:44 PM
Hi @TimeDigger ,
Thanks for your feedback.
I'm not able to reproduce this issue, could you please give me more details ?
-STM32CubeMX starting version
-are you using Windows 10, windows 7, Linux?
-if possible send me the migrated file .
Regards,
Houda
2019-01-10 10:09 AM
Hi,
-STM32CubeMX starting version
If it is asked here that what version it was before I updated STM32CubeMX to v5.0.1, I do not remember excatly. Possibly it was one of the latest releases of v4.
-are you using Windows 10, windows 7, Linux?
Windows 10
-if possible send me the migrated file.
I think this is not really relevant. Because after uptading the STM32CubeMX to v5.0.1 it has never been able to launch even once. This the problem already.
I deleted the folder of STM32CubeMX. Removed Java. Started all over again, but it did not work.
Most strangely, I have downloaded and installed from the site some of the latest releases of the previous v4 of STM32CubeMX, did not work too.
Help please !?
Best regards.
Selcuk
2019-01-19 04:04 PM
Hi, I am still not able run any verison of STM32CubeMx.
I have just tried to install it once again to see if this time I could make it succesfully. During installation, for the very fist time I pressed the "Generate an automatic installation script" button and I got the attached error massage.
I do not if this could be helpfull for my case!?
Thanks.