2019-05-28 12:13 PM
It was my hope that cubeMX bugs are constantly fixed with new releases. Unfortunately...
In the latest cubeMX generated code in FreeRTOSConfig.h file this is defined for os tick:
#define xPortSysTickHandler SysTick_Handlerwhich makes it jump into HardFault as there is nothing checks whether scheduler started or not.
WTF????
It was working correctly in previous release.
It was properly commented in FreeRTOSConfig.h:
/* IMPORTANT: This define MUST be commented when used with STM32Cube firmware,
to prevent overwriting SysTick_Handler defined within STM32Cube HAL */
/* #define xPortSysTickHandler SysTick_Handler */Then in stm32f4xx_it.c it was an ISR:
void SysTick_Handler(void)
{
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
osSystickHandler();
/* USER CODE BEGIN SysTick_IRQn 1 */
/* USER CODE END SysTick_IRQn 1 */
}And finally needed check:
void osSystickHandler(void)
{
#if (INCLUDE_xTaskGetSchedulerState == 1 )
if (xTaskGetSchedulerState() != taskSCHEDULER_NOT_STARTED)
{
#endif /* INCLUDE_xTaskGetSchedulerState */
xPortSysTickHandler();
#if (INCLUDE_xTaskGetSchedulerState == 1 )
}
#endif /* INCLUDE_xTaskGetSchedulerState */
}
2019-08-07 7:39 AM
@GShma - You may want to review this:
http://www.nadler.com/embedded/newlibAndFreeRTOS.html
Hope that helps,
Best Regards, Dave