cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX bug for FDCAN?

Imre
Associate II

Hi ST

I am using STM32CubeMX v6.10.0 with selected MCU STM32H563ZITx.
When configuring FDCAN1 I may have found a bug in the tool. The below two Nominal Time Seg1 and Seg2 say that the lowest value is "2" and the tool is limiting setting it to "1" which I think is a valid setting.

Imre_0-1707302997348.png

Imre_1-1707303014423.png

The RM0481 Rev 1 says that the minimum value that is interpreted by the hardware of that value is "1" (when register segment is set to "0")

Imre_2-1707303308710.png

Can someone please verify my findings?

Br
Imre

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Yes according to the RM:  NTSEG1 is in the range [0:255] and NTSEG2 ins the range [0:127].

In the HAL there is a substraction to meet these ranges:

  hfdcan->Instance->NBTP = ((((uint32_t)hfdcan->Init.NominalSyncJumpWidth - 1U) << FDCAN_NBTP_NSJW_Pos) | \
                            (((uint32_t)hfdcan->Init.NominalTimeSeg1 - 1U) << FDCAN_NBTP_NTSEG1_Pos)    | \
                            (((uint32_t)hfdcan->Init.NominalTimeSeg2 - 1U) << FDCAN_NBTP_NTSEG2_Pos)    | \
                            (((uint32_t)hfdcan->Init.NominalPrescaler - 1U) << FDCAN_NBTP_NBRP_Pos));

So, to me, in CubeMx the ranges should be:

  • BS1: [1:256] 
  • BS2: [1:128]

I'm raising this behavior internally and get back to you with feedback

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

Yes according to the RM:  NTSEG1 is in the range [0:255] and NTSEG2 ins the range [0:127].

In the HAL there is a substraction to meet these ranges:

  hfdcan->Instance->NBTP = ((((uint32_t)hfdcan->Init.NominalSyncJumpWidth - 1U) << FDCAN_NBTP_NSJW_Pos) | \
                            (((uint32_t)hfdcan->Init.NominalTimeSeg1 - 1U) << FDCAN_NBTP_NTSEG1_Pos)    | \
                            (((uint32_t)hfdcan->Init.NominalTimeSeg2 - 1U) << FDCAN_NBTP_NTSEG2_Pos)    | \
                            (((uint32_t)hfdcan->Init.NominalPrescaler - 1U) << FDCAN_NBTP_NBRP_Pos));

So, to me, in CubeMx the ranges should be:

  • BS1: [1:256] 
  • BS2: [1:128]

I'm raising this behavior internally and get back to you with feedback

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Hello,

Internal ticket submitted to treat this issue (172861) and the bug is confirmed. It will be fixed in one of the coming versions of CubeMx.

Thank you for raising the issue.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Issue fixed in the latest version of CubeMx V6.11.0 already available on the web.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.