cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 6.0.0 released

Nawres GHARBI
ST Employee

What is new in STM32CubeMX V6.0.0?

 Added the support of new part numbers in the STM32G4 Series: STM32G491K(C-E)Ux, STM32G491C(C-E)Ux, STM32G491C(C-E)Tx, STM32G491REYx, STM32G491R(C-E)Tx, STM32G491R(C-E)Ix, STM32G491M(C-E)Sx, STM32G491M(C-E)Tx, STM32G491V(C-E)Tx, STM32G4A1KEUx, STM32G4A1CEUx, STM32G4A1CETx, STM32G4A1REYx, STM32G4A1RETx, STM32G4A1REIx, STM32G4A1MESx, STM32G4A1METx, and STM32G4A1VETx

 Added the support of new part numbers in the STM32H7 Series: STM32H723x, STM32H725x, STM32H730x, STM32H733x and STM32H735x

 Added the support of one new part number in the STM32F4 Series: STM32F479IIHx

 Added the support of three new part numbers in the STM32F7 Series: STM32F723V(C-E)Tx and STM32F733VETx

 Added the support of new part numbers in the STM32L0 Series: STM32L031C4Ux, STM32L041C6Ux, STM32L051C(6-8)Ux, STM32L052C(6-8)Ux, STM32L053C(6-8)Ux, STM32L062C8Ux, STM32L063C8Ux, STM32L071C8Ux, STM32L082KBUx and STM32L083RBTx

 Added the support of new part numbers in the STM32L1 Series: STM32L162QCHx, STM32L162VDYxX and STM32L162ZCTx  Added the support of new part numbers in the STM32L4 Series: STM32L496VGTxP, STM32L496VGYxP and STM32L4A6VGTxP

 Added the support of one new part number in the STM32WB Series: STM32WB55VYYx

 Added the support of new boards: NUCLEO-G491RE, STM32H735G-DK, NUCLEO-H723ZG, NUCLEO-WB55RG, B-L462E-CELL1, B-L4S5I-IOT01 and STM32MP157F-EV1

 Added the video tutorials feature to access video tutorials on various STM32CubeMX features

 Added the support of an Example Selector that enables example filtering among several parameters

 Added the support of PCC for the STM32L5xQ part numbers with SMPS

 Software Packs: – User interface enhancements with simplified access to Software Pack installation and component selection from the Pinout&Configuration view and to Software Pack documentation from the Component Selector window – Implementation aligned with Arm® CMSIS-Pack 1.6.3 revision

 Added a graphical tool, named STM32PackCreator and installed with STM32CubeMX in the Utilities folder. It allows pack developers to create Software Packs and STM32Cube Expansion packages enhanced for STM32CubeMX. It can be launched from the ST Tools tab found in the STM32CubeMX Tools view.

STM32CubeIDE toolchain:

 It is functional only with a Java 8 64-bit Java Virtual Machine.

Example Selector:

 The feature is functional only for the examples related to the STM32F4, STM32F7, STM32G0, STM32G4, STM32H7, STM32L5 and STM32WB Series

Software Packs:

 When a pack is disabled, generated files are not removed from the project

– Workaround: remove these files manually

 Possible issue with component dependencies in the Additional Software components selection window

– Workaround: click on the Refresh button from the Embedded Software Packages Manager

 When using the GNSS pack, users must not migrate their project from 3.x to 4.0.0

 Functionalities not supported:

– maxInstances, isDefaultVariant, generator attributes of the component element

– Dtz, Ddsp, Dsecure attributes of the condition element

– repository element – tag and url attributes of a release element

– dominate element

– public attributes for the file element

– preIncludeLocal and preIncludeGlobal file category attributes

– Pre_Include_Local_h element

– Pre_Include_Global_h element

– Pack components where attribute values come with a "." character

Link

https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/stm32cubemx.html

1 REPLY 1
RJ..1
Associate

Installed the very first time a STM-Software. CubeMX only shows the Startscreen, then nothing. No Program, no entry in Windows-Taskmanager, nothing