cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 5.0 regenerate code with SW4STM32 and missing floder

cchen.12
Associate III

I update my Stm32CubeMX to 5.0, and open an old project , regenerate the code with ToolChain SW4STM32

I have some floder missing, I must recreate the floder and copy the files into it.

The old version of Stm32CubeMX is OK.

Is there a solution?

1 ACCEPTED SOLUTION

Accepted Solutions
WBOUG
Senior

Hi @cchen.1​ 

I'm OK with you and it will be corrected in the next next version.

Best Regards.

Wael.

View solution in original post

2 REPLIES 2
WBOUG
Senior

Hi @cchen.1​ 

I'm OK with you and it will be corrected in the next next version.

Best Regards.

Wael.

I have updated the Stm32CubeMX to 5.1.0 but the problem still exist. If I drag a file into a src folder .There are two options. It’s OK when I select option. But the file link will missing after regenerate the code with ToolChain SW4STM32 when I select option. If the folder contains files only. The folder will be deleted also. 從 Windows 10 的郵件傳�? 寄件者: ST Community 傳�?時間: 2018年12月21日 下�?� 05:43 收件者: f054799@gmail.com 主旨: wael.bougattaya1.5433181036799783E12 mentioned you in an answer to:STM32CubeMX 5.0 regenerate code with SW4STM32 and missing floder Hi @f0547991.545207255917735E12​    I'm OK with you and it will be corrected in the next next version.   Best Regards. Wael.               wael.bougattaya1.5433181036799783E12 (STMicroelectronics) Hi @f0547991.545207255917735E12 (Ching Gu Electronics CO. LTD.)​    I'm OK with you and it will be corrected in the next next version.   Best Regards. Wael.       or reply to this email             Replying to       f0547991.545207255917735E12 (Ching Gu Electronics CO. LTD.) asked a question. Wednesday, December 19, 2018 12:33 AM STM32CubeMX 5.0 regenerate code with SW4STM32 and missing floder I update my Stm32CubeMX to 5.0, and open an old project , regenerate the code with ToolChain SW4STM32   I have some floder missing, I must recreate the floder and copy the files into it. The old version of Stm32CubeMX is OK.   Is there a solution?               wael.bougattaya1.5433181036799783E12 (STMicroelectronics) Hi @f0547991.545207255917735E12 (Ching Gu Electronics CO. LTD.)​    I'm OK with you and it will be corrected in the next next version.   Best Regards. Wael.   Friday, December 21, 2018 1:43 AM               You're receiving emails when someone "Mentions me in a comment."   To change or turn off ST Community email, log in as f054799@gmail.com.st.   STMicroelectronics N.V.