I have updated the Stm32CubeMX to 5.1.0 but the problem still exist.
If I drag a file into a src folder .There are two options.
It’s OK when I select option.
But the file link will missing after regenerate the code with ToolChain SW4STM32
when I select option.
If the folder contains files only.
The folder will be deleted also.
從 Windows 10 的郵件傳�?
寄件者: ST Community
傳�?時間: 2018年12月21日 下�?� 05:43
收件者: f054799@gmail.com
主旨: wael.bougattaya1.5433181036799783E12 mentioned you in an answer to:STM32CubeMX 5.0 regenerate code with SW4STM32 and missing floder
Hi @f0547991.545207255917735E12 I'm OK with you and it will be corrected in the next next version. Best Regards. Wael.
wael.bougattaya1.5433181036799783E12 (STMicroelectronics)
Hi @f0547991.545207255917735E12 (Ching Gu Electronics CO. LTD.)
I'm OK with you and it will be corrected in the next next version.
Best Regards.
Wael.
or reply to this email
Replying to
f0547991.545207255917735E12 (Ching Gu Electronics CO. LTD.) asked a question.
Wednesday, December 19, 2018 12:33 AM
STM32CubeMX 5.0 regenerate code with SW4STM32 and missing floder
I update my Stm32CubeMX to 5.0, and open an old project , regenerate the code with ToolChain SW4STM32
I have some floder missing, I must recreate the floder and copy the files into it.
The old version of Stm32CubeMX is OK.
Is there a solution?
wael.bougattaya1.5433181036799783E12 (STMicroelectronics)
Hi @f0547991.545207255917735E12 (Ching Gu Electronics CO. LTD.)
I'm OK with you and it will be corrected in the next next version.
Best Regards.
Wael.
Friday, December 21, 2018 1:43 AM
You're receiving emails when someone "Mentions me in a comment."
To change or turn off ST Community email, log in as f054799@gmail.com.st.
STMicroelectronics N.V.