cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE doesn't save clock configuration

matteverze
Associate II

Hi, I'm facing a problem with the Clock Configuration tab with the latest version of the STM32CubeIDE. In fact, every time I open the ioc file, there is an error with the SMPS Clock Mux on the STM32WB board I'm using. I correct and generate code and saved but when I open the file again the error is still there. I'm using the latest version of the Cube.

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions

@SofLit wrote:

I reproduced the behavior.

I will escalate the issue internally and get back to you as soon as I have an answer/feedback.

Internal ticket 190817 for follow-up.


Issue fixed in CubeMx V6.13.0

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
SofLit
ST Employee

Hello,

What error is displayed? Could you please share your ioc file?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
matteverze
Associate II

Hi, 

I share some pictures of the problem. To correct the problem, I change the SMPS Clock Mux to HSE as shown in the tutorial. However, when I generate the code and save it goes to HSI again. I attach also the ioc.

Thanks.

Screenshot 2024-09-11 154740.png

Screenshot 2024-09-11 154745.png

Screenshot 2024-09-11 154756.png

   

SofLit
ST Employee

I reproduced the behavior.

I will escalate the issue internally and get back to you as soon as I have an answer/feedback.

Internal ticket 190817 for follow-up.

Thank you for your patience.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@SofLit wrote:

I reproduced the behavior.

I will escalate the issue internally and get back to you as soon as I have an answer/feedback.

Internal ticket 190817 for follow-up.


Issue fixed in CubeMx V6.13.0

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.