cancel
Showing results for 
Search instead for 
Did you mean: 

SOLVED: CubeMX 5.1.0 re-generated project for SW4STM32 linker script *.LD file is empty. GONE: with CubeMX 5.2

G_1
Associate II

CubeMX 5.1.0 and STM32F302 every time a project is re-generated the

STM32F302R8Tx_FLASH.ld file is empty.

This discussion is locked. Please start a new topic to ask your question.
19 REPLIES 19
G_1
Associate II

Hi @ Nesrine,

thx, but where can i download the 5.2.0 ?

There is only the selection of older versions!

And the update function will not find a new version?

So long

G

Hi, please see projects made in SW4STM32 v 2.8.1 using CubeMX v 5.1.0rc6 HAL F1 v 1.7.0

And another one made in SW4STM32 v 2.8.1 using CubeMX v 5.1.0rc6 HAL F1 v 1.7.0

Hi @fronders​ 

Will be fixed next release.

Best regards.

Nesrine

Mark Shoe
Senior

This happens me many times on different cpu's. The empty file problem started from version 5.1.0.

It is a problem for me because I made changes to the sections for the bootloader.

Hi @Community member​ 

This is a bug that has been fixed in the new version of STM32CubeMX 5.2.0.

Best regards,

Nesrine

Rutr
Associate

Also I and my friends have this problem. Cube eclipse plugin version 5.1.0.

After re-geneerate the linker file is empty. STM32 F103C8, Windows 10 x64

Is there cube eclipse plugin in version 5.2 ?

G_1
Associate II

Hi,

use 5.2 and the error is gone.

There are three ways to get the update.

Nice day and regards.

G_1
Associate II

Hi

use 5.2 and the error is gone. There are three ways to do the update.

So long and THX