cancel
Showing results for 
Search instead for 
Did you mean: 

SMPS on the STM32H747XI

Hal56-GCI
Associate II

I have created a project for the STM32H747I-DISCO and have deadlocked the MCU twice. a BIG thanks to ST for not having ANY warning about this.

 

The DISCO board comes configured to default to SMPS mode. The project I created, without any warnings, defaulted to LDO mode. I corrected the problem using the process described in UM2411, section 5.2.3 only to go right back into the deadlock condition when downloading code.

I now know that I must set the power mode to SMPS but I cannot find this setting in CubeMX.

 

I am using CubeIDE v1.17.0. Where is the power settings for LDO and SMPS?????

3 REPLIES 3
SofLit
ST Employee

Most probably it's an issue pointed out by @Tesla DeLorean 

There is a limitation in CubeMx 6.13.CubeIDE v1.17.0. It will be fixed as soon as possible.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

>>I have created a project for the STM32H747I-DISCO and have deadlocked the MCU twice. a BIG thanks to ST for not having ANY warning about this.

I think I immediately bricked my H747I-DISCO about 7 years ago, and after doing the BOOT0 R192, had suggested a BOOT0 switch somewhere accessible, way back then. Same issue with the H745 / H750 DISCO's. I recollect there being an STM32 Cube Programmer "Access Port" trick too, but I don't recollect how that worked. These days I solder a right-angle jumper on the NUCLEO-144 H7 boards between VDD and BT0

https://community.st.com/t5/stm32cubeprogrammer-mcus/error-to-connect-to-target-stm32h747i-disco/m-p/294136

https://community.st.com/t5/stm32-mcus-boards-and-hardware/location-of-stm32h747i-disco-boot0-pin/td-p/156886

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..