cancel
Showing results for 
Search instead for 
Did you mean: 

SMPS Configuration

IP.2
Associate II

Using STM32CubeMX Version 6.11.1 for code generation of STM32U545RETxQ LQFP64.

When pressing "Generate Code" there is a message recommending SMPS setting from the PWR menu.

However, no SMPS there and not anywhere in the configuration menu. (Attached)

Any idea?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @IP.2 

To configure the SMPS you need to go to: Power and Thermal>PWR>Low Power and check the box Power Saving mode. After that, on the configuration tab go to Power Saving>System power supply and you can configure the Power Regulator to LDO or SMPS:

STTwo32_0-1733471515472.png

PS: Make sure to use the last version of the STM32CubeMX (V6.13.0).

 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @IP.2 

To configure the SMPS you need to go to: Power and Thermal>PWR>Low Power and check the box Power Saving mode. After that, on the configuration tab go to Power Saving>System power supply and you can configure the Power Regulator to LDO or SMPS:

STTwo32_0-1733471515472.png

PS: Make sure to use the last version of the STM32CubeMX (V6.13.0).

 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.