2019-02-26 11:54 AM
In CubeMX when choosing fatfs middleware it seems to require a gpio pin. Is that just a limitation in CubeMX?
Basically is there a reliable software card detect mechanism using the existing SDMMC lines (4 pin SD card) or must an extra gpio pin be used to the sd card detect pin?
Thanks,
-Fred
2019-02-26 1:09 PM
As the sockets pretty much all have a mechanical switch mechanism, people tend to focus on those. ST has some of their board examples use that to generate an EXTI interrupt.
The example code is mostly provided as a demo of functionality, not something that would meet commercial requirements for fit/finish.