2018-12-11 4:07 AM
I use the CMSIS wrapper for FreeRTOS generated by CubeMX. This Project was generated about 4 month ago with the current version at that time. I didn't find this bug in forums so I'll ask here.
In *osPoolAlloc() the array of pool entries will be search for a free spot. If it's found in the markers-array, the corresponding memory pointer is returned. I think to speed up sucessive allocations, a currentIndex is saved. If I interpreted the code right, the search should start at currentIndex and wrap around the markers-array.
E.g. is the length is 5 (0, ..., 4) and currentIndex is 2, the order should be 2, 3, 4, 0 and finally 1.
The generated code looks like this:
for (i = 0; i < pool_id->pool_sz; i++) {
index = pool_id->currentIndex + i;
if (index >= pool_id->pool_sz) {
index = 0;
}
// actual logic
}What happens is instead of wrapping the index, it will be set to 0. In the example the sequence 2, 3, 4, 0, 0 will be generated. This fixes the behaviour:
for (i = 0; i < pool_id->pool_sz; i++) {
index = (pool_id->currentIndex + i) % pool_id->pool_sz;
// actual logic
}Can someone verify this and check, if this wasn't fixed in the meantime?
Thanks!
2018-12-13 12:59 AM
Hello @FStut,
Thank you for reported this issue. This is already raised internally for fix as a better implementation would be:
index = (pool_id->currentIndex + i) % pool_id->pool_sz;without resetting the index to '0'.
Kind Regards,
Imen