2019-04-24 1:28 AM
I am using the eval board STM32L4R9I-EVAL.
The generated code failde in OCTOSPI1_Init/ HAL_OSPI_AutoPolling:
it runs by
if ((hospi->State == HAL_OSPI_STATE_CMD_CFG) && (cfg->AutomaticStop == HAL_OSPI_AUTOMATIC_STOP_ENABLE))
{
.....
}
else
{
..........
}
into HAL_Error.
does any one know why?
CubeMX: V5.1.0
Package for STM32L4: V1.13.0
Octospi2 on Hyperram works fine.
2019-04-25 11:48 PM
I tried the exsample in OSPI_NOR_MemoryMapped in STM32Cube_FW_L4_V1.13.0\Projects\STM32L4R9I-EVAL\Examples\OSPI\ long time ago, they work fine.
the example OSPI_NOR_MemoryMapped in STM32Cube_FW_L4_V1.14.0\Projects\STM32L4R9I-EVAL\Examples\OSPI\ works fine without any errors also.
The example has another structure and call first a few extra commands (enable write cmd and autopolling configuration command) before calling the function HAL_OSPI_AutoPolling. Now I hope with new release of L4-Packages cubemx could generate code which is usable. otherwise i have to modify it every time when i use cubemx to regenrate code.
I have the same problem with generated code für hyperram on octospi port 2. The generated code didn't work because it called the function HAL_OSPI_MemoryMapped to early, it should call it after the hyperbus is configured and the chip is set into memory-mapped mode, so i have to modify this section every time i regenerate code using cubemx.
How to report this to ST so it get corrected in the next release?
thanks