cancel
Showing results for 
Search instead for 
Did you mean: 

missing "INITIALIZE ALL PERIPHERALS IN DEFAULT MODE" with STm32 Cube IDE 1.17.0

PG29
Associate

Hi, 

I just updated my version of STM32Cube IDE (1.17.0) on my PC, and I miss the "INITIALIZE ALL PERIPHERALS IN DEFAULT MODE" when I start a new project with my NUCLEO-H723ZG board. Instead of that, I have a new popup, "Board Project Options" with only HMI things, and it results in the ETH not being initialized for example. 

Maybe I have missed some settings? Is the "INITIALIZE ALL PERIPHERALS IN DEFAULT MODE" mode still available in this version?

Thank you for your help

1 ACCEPTED SOLUTION

Accepted Solutions
Mahmoud Ben Romdhane
ST Employee

Hello @PG29 ,

First let me thank you for posting and welcome to the ST Community.

It is a normal behavior, in fact Start From Board is a functionality of STM32CubeMX that simplifies the creation of a project on a board.

In this case, the project can quickly be generated and uploaded to a board.

For more information, I suggest that you take a look at this ST Wiki.

It explains what is Start From Board feature, how to use it through a detailed example and the supported boards.

Best Regards.

Mahmoud

View solution in original post

1 REPLY 1
Mahmoud Ben Romdhane
ST Employee

Hello @PG29 ,

First let me thank you for posting and welcome to the ST Community.

It is a normal behavior, in fact Start From Board is a functionality of STM32CubeMX that simplifies the creation of a project on a board.

In this case, the project can quickly be generated and uploaded to a board.

For more information, I suggest that you take a look at this ST Wiki.

It explains what is Start From Board feature, how to use it through a detailed example and the supported boards.

Best Regards.

Mahmoud