2019-04-08 7:36 AM
Hey,
I´m confused why i can not use Pin PD2 on Cube MX on the Nucleo Board L433RC even though it should actually exist because it exist when you select another STM32L433.
Without that Pin, i can´t use SDMMC. If i select for example the STM32L433RCTx, there is the Pin PD2. But if i try to use it with the Nucleo it wont work.
Any suggestions?
Solved! Go to Solution.
2019-04-10 12:43 AM
Hello @SWend
This is reported internally for further check.
Best Regards,
Khouloud