Skip to main content
denis2
Associate
May 16, 2017
Question

Missing ''busy'' state handling in custom USB HID code generated by MX

  • May 16, 2017
  • 5 replies
  • 1410 views
Posted on May 16, 2017 at 12:51

I'm using STMCubeMX 4.21.0 to generate custom USB HID project. My device needs to send frequent HID reports, therefore it calls USBD_CUSTOM_HID_SendReport every 1-10ms.

This function always returns USBD_OK, even if previous report is not transmitted - in this case it just ignores new report.

It becomes a problem because there is no way for user code to check if data was successfully transmitted or another attempt is required.

I've implemented a local workaround in this function: it returns USBD_BUSY when hhid->state == CUSTOM_HID_BUSY

But this change is not in user modifiable area, therefore this change is lost on every project re-generation in CubeMX.

Am I missing something, is there any other good way to work around this issue?

#cubemx-usb-hid
This topic has been closed for replies.

5 replies

ST Technical Moderator
May 17, 2017
Posted on May 17, 2017 at 14:02

Hi

Tyurin.Denis_Mikhail

,

Please attach your .ioc file.I shared thisissue internally with our CubeMx team for further check and investigation.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
denis2
denis2Author
Associate
May 17, 2017
Posted on May 17, 2017 at 14:14

Sure, here is the link to ioc file:

https://raw.githubusercontent.com/denis-m-tyurin/IRtoUSB/master/Firmware/IR_TO_USB/IR_TO_USB.ioc

Zheng Liang
Associate III
October 25, 2017
Posted on October 25, 2017 at 13:59

This still exists in v4.1, my thought is smae with

HAMMI.Imen

‌, there need a busy state with return to check whether the data is transmitted

successfully.

0690X00000608i6QAA.png

Pavel A.
February 24, 2018
Posted on February 24, 2018 at 02:18

I did this too for my device project on STM32F072.

-- pa

stm32cube-t
ST Employee
February 23, 2018
Posted on February 23, 2018 at 18:53

Hello,

Please note this is not an STM32CubeMX issue but a USB device library issue. The fix will be available with the next version of the library, that is delivered as part of the STM32Cube MCU embedded software packages.

Best regards.