cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N645Z0 Ethernet Configuration Support in STM32CubeMX

modecs
Associate II

I am currently evaluating the

for use with 1000Base-T Ethernet and am attempting to configure the peripherals using STM32CubeMX. While following the same process as with other STM32 chips, I was unable to find the Ethernet configuration under Pinout & Configuration -> Connectivity. Could you kindly advise where I should configure the Ethernet settings?

Thank you for your assistance.

1 ACCEPTED SOLUTION

Accepted Solutions
Ghofrane GSOURI
ST Employee

Hello @modecs 

Thank you for your contribution.

ETH should be available for STM32N645Z0, according to*DS14791 Rev. 9, Table 18, which indicates Ethernet signal support for the VFBGA142 package.

For RMII mode, the supported signals are

ETH1_MDC on B12, ETH1_MDIO on K1, ETH1_CLK on K3, ETH1_RMII_REF_CLK on M2, ETH1_RMII_CRS_DV on K2, ETH1_RMII_TX_EN on N2, ETH1_RMII_TXD0 on P1, ETH1_RMII_TXD1 on N3, ETH1_RMII_RXD0 on L2, and ETH1_RMII_RXD1 on M1.

A ticket #0062266  has been escalated to the development team to investigate and correct this behavior.

I will keep you posted with updates.

THX

Ghofrane 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Ghofrane GSOURI
ST Employee

Hello @modecs 

Thank you for your contribution.

ETH should be available for STM32N645Z0, according to*DS14791 Rev. 9, Table 18, which indicates Ethernet signal support for the VFBGA142 package.

For RMII mode, the supported signals are

ETH1_MDC on B12, ETH1_MDIO on K1, ETH1_CLK on K3, ETH1_RMII_REF_CLK on M2, ETH1_RMII_CRS_DV on K2, ETH1_RMII_TX_EN on N2, ETH1_RMII_TXD0 on P1, ETH1_RMII_TXD1 on N3, ETH1_RMII_RXD0 on L2, and ETH1_RMII_RXD1 on M1.

A ticket #0062266  has been escalated to the development team to investigate and correct this behavior.

I will keep you posted with updates.

THX

Ghofrane 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.