2017-01-27 1:22 AM
There seems to be a problem downloading the stm32cube_fw_l0_v180 from within the newest STM32Cube. See the attached screenshots. It seems to me it tries to unzip 'stm32cube_fw_l0_v180.zip' to a folder named 'stm32cube_fw_l0_v180.zip' which obviously does not work. Does anyone else have this problem?
#stm32cube_fw_l0_v180 #stm32cubemx2017-01-27 4:13 AM
Ok, so I tried this again and now a couple of hours later it works. But I don't like the stability of this. Sometimes it works, sometimes i doesn't. Is there a logfile somewhere with some more verbose description of this error?
2017-01-27 4:43 AM
Hello
Gullberg.Daniel
,We could not reproduce the same issue.
The log file is provided under the path below: 'C:\Users\<Username>\.stm32cubeMX'
Khouloud
2017-02-01 9:03 AM
Ok, the tail of my logfile looks like this, mentioning 'Error Problem during Download of File' a couple of times:
2017-01-27 08:51:47,506 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...
2017-01-27 08:51:47,508 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 08:51:58,394 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_l0_v180.zip2017-01-27 08:52:34,723 [ERROR] ServerAccessManage:256 - Error Problem during Download of File : stm32cube_fw_l0_v180.zip.2017-01-27 08:52:34,731 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 08:52:34,732 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 08:52:40,656 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_f7_v160.zip2017-01-27 08:55:53,554 [ERROR] ServerAccessManage:256 - Error Problem during Download of File : stm32cube_fw_f7_v160.zip.2017-01-27 09:20:41,648 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 09:20:41,668 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 09:20:45,180 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 09:20:45,181 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 09:20:46,597 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_l0_v180.zip2017-01-27 09:21:22,158 [ERROR] ServerAccessManage:256 - Error Problem during Download of File : stm32cube_fw_l0_v180.zip.2017-01-27 10:00:55,929 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 10:00:55,940 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 10:00:59,256 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 10:00:59,258 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 10:01:01,011 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_l0_v180.zip2017-01-27 10:01:36,947 [ERROR] ServerAccessManage:256 - Error Problem during Download of File : stm32cube_fw_l0_v180.zip.2017-01-27 10:01:36,952 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 10:01:36,954 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 10:01:37,866 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_f7_v160.zip2017-01-27 10:05:19,186 [ERROR] ServerAccessManage:256 - Error Problem during Download of File : stm32cube_fw_f7_v160.zip.2017-01-27 10:05:22,599 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 10:05:22,606 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 10:05:28,268 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 10:06:02,726 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 10:06:02,728 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 10:06:03,543 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_l0_v180.zip2017-01-27 10:06:26,249 [INFO] FileExtend:164 - Unzip File : stm32cube_fw_l0_v180.zip2017-01-27 10:06:26,253 [INFO] FileExtend:173 - Standard Deflate2017-01-27 10:07:46,320 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 10:07:46,332 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 10:09:03,035 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 10:09:06,248 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 10:09:06,249 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 10:09:07,731 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_l0_v180.zip2017-01-27 10:09:44,036 [ERROR] ServerAccessManage:256 - Error Problem during Download of File : stm32cube_fw_l0_v180.zip.2017-01-27 10:09:45,496 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 10:09:45,512 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 10:09:51,852 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 10:09:51,854 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 10:09:52,773 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_l0_v180.zip2017-01-27 10:10:12,784 [INFO] FileExtend:164 - Unzip File : stm32cube_fw_l0_v180.zip2017-01-27 10:10:12,786 [INFO] FileExtend:173 - Standard Deflate2017-01-27 10:18:14,767 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 10:18:14,773 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 10:18:42,288 [INFO] About:247 - Version : DB.4.0.190Db Path : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX//db/2017-01-27 12:58:36,994 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 12:58:39,677 [INFO] FileExtend:164 - Unzip File : stm32cube_fw_l0_v180.zip2017-01-27 12:58:39,678 [INFO] FileExtend:173 - Standard Deflate2017-01-27 12:59:38,049 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 12:59:38,060 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 13:10:47,064 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 13:10:47,065 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 13:10:48,678 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_f7_v160.zip2017-01-27 13:14:07,327 [ERROR] ServerAccessManage:256 - Error Problem during Download of File : stm32cube_fw_f7_v160.zip.2017-01-27 13:14:10,092 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 13:14:10,104 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread2017-01-27 13:14:35,784 [INFO] ServerAccessManage:517 - Connection to HTTP Server ...2017-01-27 13:14:35,785 [INFO] ServerAccessManage:553 - System Protocol : DIRECT2017-01-27 13:14:36,674 [INFO] ServerAccessManage:147 - Download File stm32cube_fw_f7_v160.zip2017-01-27 13:17:53,645 [INFO] FileExtend:164 - Unzip File : stm32cube_fw_f7_v160.zip2017-01-27 13:17:53,646 [INFO] FileExtend:173 - Standard Deflate2017-01-27 13:19:37,575 [INFO] LoadServerPackagesThread:114 - End of LoadServerPackage Thread2017-01-27 13:19:37,596 [INFO] CheckServerUpdateThread:99 - End of CheckServer Thread