cancel
Showing results for 
Search instead for 
Did you mean: 

Is this the correct site to raise problems with CubeMX?

JCool.1
Associate II
 
12 REPLIES 12
 

Hi @JCool.1​ 

Thanks for the detailed file, generally this type of problem is caused by a java version installed which is not supported by CubeMX.

In fact, the minimum JRE version is 1.8_45 (known limitation with 1.8_251), also the version 11 is supported, for the versions 7, 9, 10, 12 and upper, they are not supported.

Can you please share your log file after facing the issue? (you can find .log file is under \Users\..\.stm32cubemx).

Thanks, Khouloud

Hi Khouloud
I have installed the latest version of Java (1.8 update 281) but the problem is unchanged.
With regards
Jim Cooling