cancel
Showing results for 
Search instead for 
Did you mean: 

Interesting http iap in STM32CubeMX

MJere.1
Associate

STM32F4x7 in-application programming (IAP) over Ethernet based on LwIP TCP/IP stack (AN3968), it is possible to realize this with stm32cubemx. Maybe there are manuals like this done through STM32CubeMX?

2 REPLIES 2

Hello MJere.1,

Unfortunately there is not an Application Note detailing how to create an "STM32F4x7 IAP over Ethernet based on LwIP TCP/IP" project using STM32CubeMX, but "STM32Cube Ethernet IAP example" User Manual may helps you: https://www.st.com/resource/en/user_manual/dm00103145-stm32cube-ethernet-iap-example-stmicroelectronics.pdf.

You can also find multiple examples in New project window - Example selector, that allows to start a new project from a selected example.

0693W000004JaKCQA0.png 

Regards,

Khouloud.

MJere.1
Associate

Yes, I know this example, this example does not have an ioc configuration file. The problem is that there is a project with an ioc file and a working device, I need to make it have the ability to update via the web interface (for example: routers). Judging by this documentation https://www.st.com/resource/en/user_manual/dm00103145-stm32cube-ethernet-iap-example-stmicroelectronics.pdf such an option is available, I will try to look.

Thanks for helping me,

 Regards, Mark :)