cancel
Showing results for 
Search instead for 
Did you mean: 

I2C speed problems

JonConesa
Associate III

Hi everyone,

I’m currently working on an I2C communication setup using the Nucleo-H753ZI DK but the cubeMx document is for the STM32H743BIT (the MCU for my custom board) and aiming to run it in Fast Mode (400 kHz). However, when configuring the I2C clock speed to 400 kHz, the CLK signal becomes unstable, as shown in the attached image.

JonConesa_0-1741626901002.png

To ensure the setup is functioning correctly, I ran tests with I2C configured at 100 kHz, and the communication works perfectly in that case.

 

I’ve also included an image of the system clock configuration in case there’s something that could be optimized.

JonConesa_1-1741627197068.png

JonConesa_2-1741627277291.png

JonConesa_3-1741627293171.png

 

 

Does anyone know what might be causing the instability in the CLK signal, preventing proper communication at 400 kHz?

 

Thanks in advance for your help!

22 REPLIES 22

No the SDA and SCL lines at the PCA are 3mA

padawan_0-1741696289956.png

With 5V on pullup you will burn your cpu.

And 

 

padawan_3-1741696745217.png

cause your 5V will go over the pullup to the internal pullup to the vcc of
the CPU. -> burn

padawan

 

 

 

 

 


@Ozone wrote:

> For the pull-up, I am using 5V.

A very bad idea.
You must use 3.3V. If the I2c slave(s) are 5V, use level shifters.


Pulling-up to 5V for I2C is OK:

https://community.st.com/t5/stm32-mcus-products/stm32-maximium-pin-voltage-in-output-mode/m-p/764074/highlight/true#M271241

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

While you are probably correct, the app note in the linked thread recommends a Zener diode between the ext. 5V and VDD.
I suspect the (internal) protective circuitry guaranteeing the "5V tolerance" might be to blame for the large observed "parasitic" capacity.
Especially suspicious is that it almost exclusively affect the rise time. 

So, I nonetheless recommend to try pull-ups to 3.3V instead 5V.