I was trying out CubeMX for an STM32H753 part and noticed in the Clock Configuration tab that the DIVP1 drop-down can not be set to 1. Shouldn't this be possible?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-16 9:27 AM
According to the reference manual the DIVP1 field of the RCC_PLL1DIVR register should be possible to set to 0 meaning divide by 1. And in fact I have manually used this configuration in my project in order to get a 480 MHz output from PLL1 and it works fine to set this field to 0. Is this an oversight in CubeMX?
- Labels:
-
STM32CubeMX
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-16 9:41 AM
I would argue the RM is ambiguous here. Certainly the number 1 is odd. Maybe it considers a divisor of 1 not an actual divisor and so it's allowed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-16 11:10 AM
I interpreted it as meaning 1 was allowed since otherwise in the table "0000000: ....." should state "Not allowed" like it is below for 0000010. I used this setting for two different parts now (STM32H743 and STM32H753) and it works fine. 12M crystal, multiplier 40 and divisor 1 to get a 480 MHz system clock (frequency verified). This is in a project not using CMSIS or CubeMX.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-15 7:49 AM
It appears that there is an inconsistency between the reference manual and ST's peripheral library. The STM32H753 reference manual does say that you are allowed to set DIVP to 0 for a divide value of 1:
However, the comment to the function for setting the PLL1 P Coefficient says that this is not allowed on the STM32H753 family line. From stm32h7xx_ll_rcc.h:
/**
* @brief Set PLL1 P Coefficient
* @note This API shall be called only when PLL1 is disabled.
* @rmtoll PLL1DIVR P1 LL_RCC_PLL1_SetP
* @param P parameter can be a value between 2 (or 1*) and 128 (ODD division factor not supported)
*
* (*) : For stm32h72xxx and stm32h73xxx family lines.
*/
__STATIC_INLINE void LL_RCC_PLL1_SetP(uint32_t P)
{
MODIFY_REG(RCC->PLL1DIVR, RCC_PLL1DIVR_P1, (P-1UL) << RCC_PLL1DIVR_P1_Pos);
}
Hopefully ST can provide some clarification.