cancel
Showing results for 
Search instead for 
Did you mean: 

I started a project from scratch using STMCubeMx. I did not find anywaay to highligh function such as osKernelInitialize or osThreadNew or HAL_Init() in bold violet. Can anyone tell me where to find sets. Regards

FMarr.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
MM..1
Chief III

run BUILD , crossreference start working after this

Pavel A.
Super User

On the Eclipse toolbar select "toggle mark occurrences"

0693W000003RUsiQAG.jpg

I think i did not explain correctly myself. Attached two images, in the first i have the call to function in bold and violet, in the second normal. Regards Il giorno dom 13 set 2020 alle ore 16:49 ST Community ha scritto:
Build does not work Il dom 13 set 2020, 16:18 ST Community ha scritto:
FMarr.1
Associate II

Sorry for late reply. It does not help. Happens that when the files are included in the project as link the functions are highlighted in violet