cancel
Showing results for 
Search instead for 
Did you mean: 

I'm running the Ac6/Eclipse environment on a Mac with the STM32CubeMX plugin installed. I recently updated the MX to the latest and it installed 5.1.0. Is 5.4.0 not available as the plugin? In the release notes, it says the latest compatible Cube FW is

Ron Koch
Associate II

In the release notes, it says the latest compatible Cube FW is 1.24.0. But Cube FW 1.24.1 is listed at a patch. So which should I install with STM32CubeMX 5.1.0?

When I start STM32CubeMX in its perspective I get a popup with the message "This release of STM32CubeMX Eclipse Plugin cannot be used in macOS". Is this true? What release should I use on a Mac? If I click OK on the popup, everything appears to work. Does it? Can I ignore this popup?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0